You Search For : canada (46)

  1. 600 V, Aluminum Conductor, LLDPE Insulation, PVC Jacket

  2. TransPowr® ACSS/TW is a trapezoidal aluminum conductor steel-supported concentric-lay-stranded conductor. The aluminum strands are trapezoidal in shape. The wedge-shaped aluminum strands enable a more compact alignment of the aluminum wires. Conductor designs that maintain the same circular mil cross-sectional area of aluminum as a conventional round conductor result in a TW conductor that is 10 to 15 percent smaller in overall diameter. Conductor designs that maintain the same overall diameter as a conventional round conductor result in a TW conductor that has 20 to 25 percent more aluminum cross-sectional area packed in. The ACSS/TW conductors are manufactured in accordance with the requirements of the latest issue of ASTM B857. The steel strands form the central core of the conductor, around which is stranded two, three or four layers of aluminum 1350 O temper (annealed) wires. The steel core may consist of a concentric stranded cable of 7, 19 or more wires. Numerous combinations of aluminum and steel strands and layers are possible. The sizes and constructions listed on the following pages are common examples used in overhead lines. Standard ACSS/TW designs are manufactured with regular-strength Class A zinc-5% aluminum mischmetal alloy-coated steel core (/MA2).
  3. Trapezoidal All-Aluminum 1350 Concentric-Lay-Stranded

  4. All-Aluminum 1350 Conductor Concentric-Lay-Stranded

  5. Aluminum Conductor Steel-Reinforced Compact Stranded

  6. XLPE, Low-Voltage Power, 1000 V, CSA Type RWU90, Single Conductor, Aluminum

  7. XLPE, Low-Voltage Power, 1000 V CSA Type RWU90, Single Conductor, High Speed, Copper

  8. 600 V, Aluminum Conductor, XLPE Insulation, Overall PVC Jacket