The Prysmian League

INTRODUCING THE PRYSMIAN LEAGUE.

WIRE AND CABLE HEROES. KEEPING THE WORLD CONNECTED.

The Prysmian League is a team of wire & cable superheroes born out of a need for a better, more sustainable way to stay connected and dedicated to keeping all of us linked to one another and our future. Each hero’s unique abilities mirror the innovative technology behind Prysmian Group’s best-in-class wire & cables. Together, they work vigilantly around the globe to help meet the energy and communications needs of today and tomorrow. So, let’s meet the team.

PRYSMIAN
Connection is key.

As the leader, PRYSMIAN keeps the League connected. With the ability to create energy fields to connect the world using her diamond shaped ring, Prysmian leads the team of heroes that play a crucial role to link humanity to a sustainable future.

CAROL
Heroically durable. Fearlessly flexible.

CAROL uses her power of supreme flexibility and durability to keep job sites running smoothly, even in the harshest conditions. Just like Prysmian Group’s full portfolio of CAROL® flexible cords & cordsets and electronics wire & cable.

GENSPEED
Full speed ahead.

Traveling at ultra-high speed, GENSPEED is ready to meet tomorrow’s demands for even faster data. And he’s fueled by GenSPEED® datacom cable solutions, making connecting the most complex network systems easier than ever.

LIFELINE
Strength forged in fire.

LIFELINE is the hero who runs into a burning building. Like her namesake Lifeline® fire-resistive cables, she is resistant to heat and fire. She keeps vital communication and power systems up and running when needed it is needed the most.


AIRGUARD
Always be on guard.

That’s easy to do when you’re AIRGUARD with the power to create an impenetrable shield of protection. The same way AIRGUARD® armored cable systems offer protection in some of the most demanding industries from offshore drilling to chemical refining.
 


STABILOY
Flow with the current.

STABILOY can absorb electricity to give the team the power they need to tackle any job. A trick he learned from STABILOY® aluminum alloy wire & cables, distributing power across commercial, institutional and industrial construction sites everywhere.


SUNGEN
Walk in sunshine.

SUNGEN is a shining beacon of hope for tomorrow. Her ability to withstand high temperatures and harness sunlight helps her blaze a trail toward a solar-powered future. What also helps SunGen® single conductor, sunlight-resistant, photovoltaic wire.
 


ANACONDA
Steady as a rock.

ANACONDA's superhuman strength makes him the team’s muscle. A strength only equaled by Anaconda® mining cables providing unsurpassed service life in the harshest conditions.