You Search For : canada (54)

  1. The New Lifeline® Product Offering will Enhance Safety Measures within Electrical Installations throughout Canada

  2. North American manufacturers collaborate to offer a best-in-class solution for high-speed broadband infrastructure development in Canada. Learn more!
  3. The Project Proves The Group’s Dynamism in North America Market

  4. Low Voltage Utility Cables

  5. EmPowr® Link cables are intended for use in dry or wet locations for distribution of three phase medium voltage power. These cables may be installed in ducts or direct buried.
  6. 600 V, Aluminum Conductor, LLDPE Insulation, PVC Jacket

  7. TransPowr® ACSS/TW is a trapezoidal aluminum conductor steel-supported concentric-lay-stranded conductor. The aluminum strands are trapezoidal in shape. The wedge-shaped aluminum strands enable a more compact alignment of the aluminum wires. Conductor designs that maintain the same circular mil cross-sectional area of aluminum as a conventional round conductor result in a TW conductor that is 10 to 15 percent smaller in overall diameter. Conductor designs that maintain the same overall diameter as a conventional round conductor result in a TW conductor that has 20 to 25 percent more aluminum cross-sectional area packed in. The ACSS/TW conductors are manufactured in accordance with the requirements of the latest issue of ASTM B857. The steel strands form the central core of the conductor, around which is stranded two, three or four layers of aluminum 1350 O temper (annealed) wires. The steel core may consist of a concentric stranded cable of 7, 19 or more wires. Numerous combinations of aluminum and steel strands and layers are possible. The sizes and constructions listed on the following pages are common examples used in overhead lines. Standard ACSS/TW designs are manufactured with regular-strength Class A zinc-5% aluminum mischmetal alloy-coated steel core (/MA2).